EV2300
bqStudio 1.3.42 (same problem with 1.3.45)
bq40z60 eval board
connect 2 relays for automatic learning cycle
Load Control Pin = I2C.VOUT - Test ok
Charge Control Pin = HDQ.HDQ - Test ok
Charge setup = Charge is terminated when TC bit is set
Discharge Setup = Termination Voltage 2900mV
resistive load is connected
Gauge_EN = ON
FET_EN = ON
Charger_EN = ON
Unseal Full access
Start learning cycle
STATUS: Setting device to unlearned...
STATUS: Sending command RESET...
then a Window opens:
"Startup Condition Invalid
Bit: RUP_DIS must be set ON to continue"
and in left down corner of bqStudio software "No acknowledge from device" in red
how i can set this "RUP_DIS Bit?
what does this error message "No acknowledge from device"