I have a 5 VDC input and am trying to generate 3.3V @ 200 mA and -5V @ 10 mA. This is not a lot of power, but I need to have a very small footprint (< 50 mm^2) so I'm trying to minimize the size and number of converters. The outputs don't have to be isolated from the input and don't strictly speaking have to be dc/dc either, but I'm assuming that will give best efficiency. Is there a single chip that can create both outputs? Is there a better approach than using 2 DC-DC converter chips?