Hi, I have a problem with the value of Flash Update OK Cell Volt.
Flash Update OK Cell Volt = 2800 mV × Number Of Series Cells × 5000/Voltage Divider
in my case I have the following values:
*Number Of Series Cells = 6
*Voltage Divider = 16000 mV
Flash Update OK Cell Volt = 5250
But I can not put this value in the box because it is beyond the maximum value defined for the parameter.