Hello.
My customer is using TPS73701.
And Next Model is trying to use TPS73801.
Because, End Customer's request was changed "10V≦VIN".
I have gotten any questions about these product .
<Question>
1:Is Datasheet's VIN@TYP(1.9V) value a typo?
2:Why did the datasheet change the waveform range of the Load and Line transient response in the TPS737 and TPS739?
(Because I want to compare the transient response waveform in the A and B, if you be able to obtain a comparison waveform, Please pass me.)
Could you help us?
Best Regards,
Pokkun