In reviewing the TPS65950 and I came across something that needs clarification. The external inductor of the switching power supplies is specified with a minimum inductance of 0.7uH, a nominal 1uH, and a maximum of 1.3uH.
What is the implication of making the inductor greater than 1.3uH? What are the limitations? Is it a loss of efficiency, transient response or instability? This application is subject to large magnetic fields in an MRI environment for a patient monitoring. There is an investigation into using a ferrite core inductors where the nominal inductance is 10uH but when the core is saturated due to a large external magnetic field it drops to 1uH.
In my experience, most switchers don’t mind operating with larger inductors once they are in continuous mode so my only thought is that this part is designed to run in discontinuous mode only or the compensation network is borderline with low phase margin. Can I use a larger value inductor if the change the capacitor to keep the corresponding LC filter the same?
Best regards,
Shawn