This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Full H-Bridge Driver for LED sheet, 60VDC at 2A.

Hello Team,

I am working on a project to drive 2 LED light-sheets with a full H-bridge.

I need to switch 60VDC at  2A, switching frequency is 2KHz to 4KHz and minimum pulse width is 2.5us.

I need have bit more headroom on the max voltage for this as well.

I am looking for something similar to this part HIP4082 .

Could you please provide some suggestions and recommendations? 

Thanks,

Yiding