We use the LP2981-33DBVR as voltage regulator with an input from 9v until 15v and a voltage output of 3.3v. Many of our products are having problems because the regulator LP2981-33DBVR is not working with an input voltage large than 11v. We detected the regulators that failed has a serigraphy LPB3 (text over the component). We have observed that this (LPB3) is not present in the last datasheet. What is the problem with the LP2981-33DBVR with serigraphy LPB3?