This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About the absolute maximum rating of TPS7A6350-Q1

Dear, All

A customers have questions about the absolute maximum rating of TPS7A6350-Q1.
The absolute maximum ratings of other than Vin and Ven is described as 7V.
It is a question about if it exceeds this voltage temporarily in each pin.
Either can withstand even beyond this voltage using a limiting resistor if limiting the input current?
If it is possible that this device can withstand, I want you to tell me the maximum current value that can withstand.

Thanks, Masami M.