Hi,
In bq20z70, what will happen if you disable the Impedance Track feature? Can it be disabled for a while and then re-enabled without any effect? Will the Impedance Track require some sort of re-learning after it is turned on again, or is it ready to use right away?
I want to do a few test cycles in the middle of longer test run without affecting the Impedance Track state. This would be simpler if I would not have to physically remove the evaluation board from the setup.