I stumbled across something on page 93 in the data manual for the TPS65930/TPS65920 concerning oscillator startup timing for the external oscillator feeding the HFCLKIN pin. When using the CKEN pin as the enable for the oscillator, the timing diagram gives a maximum of about 5.2 to 5.3mS for the oscillator to start. Specs for all of the CMOS 1.8V oscillators I've come across so far give 10mS as the startup time. Even if the enable pin is tied to VIO (as on the BeagleBoard) that still only gives it about 6.5mS before HFCLKOUT is expected to be stable. So what am I missing here in the startup timing, or have you lot all been using some magic oscillators that start within 5mS? Or is everyone just rolling the dice and keeping their fingers crossed?
Regards,
-Jeff