This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using TPS54340 with external FET

Other Parts Discussed in Thread: TPS54340

Hi

My customer uses TPS54340 under Vin=26V,Vout=5V,Iout=3.5A.

But it is possible  fever is high, so they will use TPP54340 with external FET to suppress the fever.

Can it use this way?

If it is correct, could you tell me to use either Pch FET or Nch FET and how to connect it?

(The board space is small so buck controller don't like this application.)

Best regards,

Yokota