This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78350-R1 Technical Reference Manual Sep 2015 does not match Battery Management Studio 1.3.45 on DA Configuration

Other Parts Discussed in Thread: BQ78350-R1, BQSTUDIO, BQ78350

Hello,

I'm programming my BQ78350-R1 using battery management studio and have come across a discrepancy. In the Technical Reference Manual (page 16), the DA Configuration register is supposed to be:

Bit 7: FTEMP
Bit 6: CTEMP
Bit 5: RSVD
Bit 4: ExtAveEN
Bit 3: VAUXEN
Bit 2: VAUXScale
Bit 1: In_System_Sleep
Bit 0: Sleep

When I select the register in Battery Management Studio however, I see the following:

Bit 7: RSVD
Bit 6: RSVD
Bit 5: RSVD
Bit 4: VExtAvg_EN
Bit 3: VAUXEN
Bit 2: VAUXScale
Bit 1: CTEMP
Bit 0: Sleep



Which is correct?

  • There was a problem with the bq78350-R1 bqz file released with bqStudio v1.3.45. Try this .bqz file.

    https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/196/2766.1E9B_5F00_1_5F00_03_2D00_bq78350_5F00_R1.bqz