This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

The Icc current question of TLC59711



In my design, both the Vcc and Vled is 13V, and I set the LED current at 34mA, I find that the Icc current is more than 25mA, but in another application which the Vcc is 5V, the Icc current is 5mA only, is that normal? I can only find the curve for Icc and output current at 12V Vcc.