This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5116

Other Parts Discussed in Thread: LM5116

Hello Eric,

Sorry, What I mean that I have three LM5116 Devices for each Output

All Devices have 80VDC Input
Device 1: I need 24V Output @ 10A I will be using 2Fets Pair in Parallel to achieve 10 Amps.
Device 2: I need 48V Output @ 10A I will be using 2Fets Pair in Parallel to achieve 10 Amps.
Device 3: I need 24V Output @ 10A I will be using 2Fets Pair in Parallel to achieve 10 Amps.

VCXX is tie to GND

My problem is I am not getting Output more than 4.8V. I can send you a working schematic.
Please advise.