I have a REG101NA-3.3 which I am trying to use as a linear post-regulator on 4.5V flyback output winding.
It usually doesn't start up properly. It appears that, some time during start-up, the regulator ends up permanently asserting an open drain load discharge switch, holding the output low. It doesn't do this all the time.
If I drive in an independent 4.5V from a bench supply, the REG101NA-3.3 wakes up and works OK.
Does the REG101NA have an input OV circuit? Or an output OV circuit?
Is it possible for some circuitry in the REG101NA to get latched up, and cause it to assert its output continuously low, despite seeing valid input voltage and load current conditions?