Hi,
In a design where the quiescent current is very critical, I need to switch a voltage up to 5 V and TPS22860 appears to be the right choice.
However, the current limitation is a bit short...
Does it sound reasonable to put 2 devices in parallel?
During switching we may have a slight unbalance between the 2 for a short duration, but since the load will also be switched at the same time (could even be switched a little later on, if required) this should not be so problematic....
Any advice?
Thanks
JYL