This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25085 and ripple injection

Other Parts Discussed in Thread: LM25085

I have designed a LM25085 based Zeta converter with the "minimum ripple configuration" circuit. The circuit work fine until the converter is in continuous current mode.

Under light load, the output show a big ripple (about 800 mV) at low frequency (6 millisec period); the average voltage is 0.4V lower than that in CCM. In this situation, the behaviour is the following: the regulator generates a burst of switching cycles (for 400 microsec) that make raise the output voltage; then the switching stop and the output voltage begins to decrease until the next burst.

I think that is the topology of ripple injection circuit itself that produce this behaviour, because it can not distinguish between CCM and DCM.

Has anyone found a way to solve this drawback ?

  • Hi Matteo,
    I am not aware of any detailed analysis done for the light load behavior of a Zeta converter with COTs. You may have to play with some different ripple values and/or COUT to tweak the circuit for satisfactory performance.