Hello,
I'm considering using the BQ76200 part for a design and were looking through the datasheet. I would like to use the PCHG output for driving a MOSFET bypassing the discharge MOSFET to precharge the bulk capacitors in a motor controller connected to the battery. Figure 10 in the datasheet seems to describe exactly what I'm looking for.
The problem is that Figure 10 is a little bit ambiguous, the text and image title hints that the MOSFET should be a P-channel, but the image shows an N-channel, which is correct?