This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Energy Star Level 6 or ERP Tier II Requirement

Other Parts Discussed in Thread: UCC28704, UCC24610, UCC24630

Hi,

 

Does TI have any power IC, which can fulfil Energy Star Level 6 or ERP Tier II Requirement

Product Power Range: 120W to 200W

IC type: Separate PFC IC + DCDC IC or Combo IC, any recommendation?

 

Rgds,

Kpk

  • Poh,
    We have the UCC28704 releasing soon to meet these requirements for low power(5-30W), but not sure on high power PFC and DC/DC that meets those requirements. You will probably need synchronous rectification so check out ucc24610 and ucc24630 to assist with that.

    I'll ask the high power team to comment here too.

    Regards
    John