In a TPS7A4701 design underway here, the LDO will have +5V applied as input, but with the EN input initially false. Prior to EN being asserted true, approximately +1V will unavoidably be applied to the output. Is the LDO expected to be able to turn on (via EN being asserted) into such a load without problem?