Can BQ78PL114 and BQ76 balance two cells at a same time? In other words: Does BQ78PL114 and BQ76 transfer energy from two or more cells in single 4.9 usec pump cycle ?
For example:
If five cells are connected to BQ78PL114 and BQ76. And voltage levels as per below
Cell 1 à 3.4 V
Cell 2 à 3.6 V
Cell 3 à 3.6 V
Cell 4 à 3.4V
Cell 5 à 3.6 V
In above case cell 1 and cell 4 are imbalance by 0.2 V. As per my understanding BQ78 and BQ76 balance two cells (or more) at a same time, but I am not sure about this. So if I design circuit for 70 mAmp balance current. Average input current for cell 1 and cell 4 will be approx 70 mAmp. In other words, if AH difference for cell 1 and cell 4 is 70mAH, cell should be balance in approximate one hour.
Please respond if anybody has an experience with this issue...