Hi Everyone
I am using the BQ34Z100 EVM Module to analyse a Li-Ion battery but find that after performing a learning cycle the "Update Status" never changes to "05" and as soon as I put a load on it to discharge the state of charge instantly drop back down to 0%.
I am using:
bqStudio Version 1.3.45
bq34z100_G1_v0_16_build_17.srec
EV2300
I have attached the battery datasheet, it is a 2Cell, 7.5V ICR-18650H 2.2AH
I have also attached some of my recent logs and my gg file.
Any help would be greatly appreciated.
Christian Haynes