I have a few queries regarding the thermal pad connector TPS79901DRVR SON package.
1) I assume that the thermal pad (EXP_PAD pin-7 in the image) is electrically not connected inside the package.
Is this true?
2) As shown in the image, TPS79901DRVR powers the analog part of the system and I have two grounds in my system
a) DAC_GND
b) GND
DAC_GNd is in signal layer and available as island.
GND is the system ground plane.
Can I connect thermal pad (EXP_PAD pin-7 in the image) to the GND plane as shown above?
Kindly let me know the proper way of handling this issue.
Regards,
Binupandian S