This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP3530 with TPS65073 power sequencing question

Other Parts Discussed in Thread: TPS65073, OMAP3530

Hi,

 

I'm currently designing a OMAP3530 system, powered with a TPS65073. From the block diagrams in several data sheets (e.g. page 9 of SLVA376) I see the DCDC2 and DCDC3  enable signals tied together (which are powering VDD_CORE and VDD_MPU respectively), however page 4 of the SLVA376 document states that VDD_MPU should only be ramped up after VDD_CORE has stabilised. Is it actually OK to ramp these two voltages together, or is there something in the TPS65073 that will power these rails correctly?

 

Thanks,

 

David.