This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8556SQE-E08 Output is only 14V



Hi,

We are trying to get an output of +24V using the LP8556SQE.  We used the component values suggested in the datasheet tables (ISET = 24K programming and FSET = floating) and we are using a 15uH inductor.  We are only seeing +14V at the output.  What could be the issue here?

Also, do the GND pins (10, 11, 15 and 24) need to be connected to a different ground than GND_SW pins (3, 4), or can we connect these all together?