As the subject notes, a client of mine is having an issue where the module will cease functioning randomly and then resume regular function randomly.
The client found that this issue seems to be caused by holding PWM (pin 8) high during start up. Start up is where Vcc is being ramped up, and SKIP# (pin 1) connected to Vdd. The device seem to enter undefined state.
The client found that to solve this issue, holding PWM (pin 8) in tristate, until Vcc is stable, the issue seems to go away.
Is this expected behavior?