This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62140 input transient

Other Parts Discussed in Thread: TPS62140

Hello Team,

Can TPS62140 operate normally if Vin fluctuates from 4.2V to 12V?

Could you give me some advice?

Customer uses TPS62140 under the following conditions and device broke (between SW and GND is 0ohm).

  • Vout = 3.3V
  • Iout = 1A
  • SS time = 1.1ms
  • Cin = 10uF
  • Cout = 22uF
  • inductor = 2.2uH
  • the load of TPS62140 connect to DCDCx4

Best Regards,

Hidetoshi Matsunami