Dear Sir
Could TPS53625 support 5V input on Denverton platform
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Yes, you need a 3.3V bias rail for VDD input pin that can be generated from the 5V power input.
Please ensure you select the right Inductor and Vin/Vout capacitors for the powerstage input/output.