This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC 28070 ic not working

Other Parts Discussed in Thread: UCC28070

Hi sir ,  I m working with ucc28070 interleaved pfc ic with following specification

1) pwm frequency ----- 75Khz

2)out put power  ------- 2500W

3)efficiency -----------  95%

4)input voltage range ----  180V-265V

As per TI application note SLUA479B i did the calculation i found i required an  Duty cycle of 0.3637 . As per the formula i put all parameter its giving me negative value kindly suggest on the same issue.

    Also i did the calculations for 0.75 % duty cycle and 75 KHz frequency  and 2500W output power and kept frequency dithering disable  by connecting pin 1 to V ref (6 V) and pin 2 to GND and first do the DC testing , as i get and 75 KHz PWM waveform  @ MOSFET Gate to Source  , by giving an 0.75 V  VSense( pin no 4) and Vin AC(pin no 5)less than 0.75 .

When i start with actual ckt as my out put voltage feedback goes above 0.75 as per the IC Specification my PFC should be Enable but its didn't happen. My SS (pin 17) gets on and off .

kindly suggest on same issue also.