This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Formula of DCAP-2's Switching frequency

Guru 19645 points
Other Parts Discussed in Thread: TPS54325

Please let me know about formula of DCAP2's fsw.

【Background】

・TPS54325

・Vin:13V⇒Vout:5V/Io:0.62A

・Inductor:SPM6530T-3R3M

⇒On Webench report, fsw:583kHz

  Customer want to know why fsw been low frequency (more than expected).

Best regards,

Satoshi

  • There is no formula for the frequency.  TPS54325 uses DCAP2 control.  There is an adaptive on time controller and hysteretic off time comparator.  Together they set the nominal switching frequency.  There is no internal oscillator.  For Vout = 5 V and Vin = 13 V, characterization data suggests that you Fsw should be about 650 kHz.  I am not sure how webench calculates Fsw for TPS54325.