Hi,
My customer has questions about LMR62014.
Could you tell me about questoins?
[Questions]
- Does the LMR62014 have soft-start function?
- How much is the start-up time?
Best Regards,
tateo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
My customer has questions about LMR62014.
Could you tell me about questoins?
[Questions]
- Does the LMR62014 have soft-start function?
- How much is the start-up time?
Best Regards,
tateo
Hello,
Denislav and I have looked into the operation of this device and have realized that the output voltage rise will depend on the slew rate of the input voltage. There is no internal soft start on this device. If the input voltage was brought up slowly like Denislav has shown in the previous reply, then the output voltage will follow Vin and have a relatively slower softstart. If Vin is already on and EN is brought up externally, then the scenario I presented takes place. Here is the snapshot of that.
In addition to this, here are a few startup waveforms with different VIN slew rates.
Here is 1 ms VIN slew rate.
Here is 2.5 ms VIN slew rate
Here is 5 ms VIN slew rate
And finally here is the 10 ms VIN slew rate
We hope this answers your questions.