Hi guys, Im looking for a synchronous controller able to deliver a constant current of 5 to 10 amp to a 24v 300w haloguen projection lamp. The trick is, I need to ramp up the current from a cold filament in a controlled way and there is where the constant current powerup mode comes in. Then the lamp will operate in half intensity (pwm) and full power mode( where the pwm controller gets bypassed) and the full power of the external power supply takes over.
The selector guide is mostly directed to constant voltage or led driving but Im having trouble finding a controller suitable for the needs.
Thanks in advance.