I'm a new user for the bq76930 and have a few questions for the cell connections to the AFE. I am connecting 8 cells in series for ~32V battery. I've connected Cell 8+ to VC10, Cell 7+ to VC9 & VC8, Cell 6+ to VC7, Cell 5+ to VC6, Cell 4+ to VC5, Cell 3+ to VC4 & VC3, Cell 2+ to VC2, and Cell 1+ to VC1. Do I have the short connections correct for the inputs?
My other question is the VC5B connection. Is it the center point of the cell connections of the 8 cells, so it would connect to the filtered VC4 connection? I have a schematic started and I'm including it here.
I just noticed that my connection for D9-A should go to VC4 instead of VC5, if I'm interpreting the connections correctly.