This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problems with SoC%, BQ3060

Other Parts Discussed in Thread: GPCCHEM

Hello. 

I have a problem that SOC% is not correct. 

  • When I discharge the battery it shows SoC 0% at 13V. Before the discharge I have written 30 in CEDV register. As shown in picture below. Is this value in hex or dec? Because I thought it was HEX so I write 30 to enable automatic EDV mode and SC=1.

  • When I charge my battery it only starts to show 1% at 14V, until that value it's 0%.
  • Correct me if I am wrong but - if battery is discharged with current lower than C/32 then automatic EDV mode doesn't work right?

I added my battery GG file and discharge and charge logs.wrongSOC.zip