This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM43603 - High resistance value for Webench interactive design

Other Parts Discussed in Thread: LM43603-Q1

HI,

I use the webench to have a recommended circuit whit simulation of the LM43603-Q1.  My main entry is 12.3V for Vin Min, 16 V for Vin max et 5V@2.3A for the output.  For that, I got a value of 1 MOhm Rfbt and 255KOhm.  Is not a little bit high.  

On my side, I begin a design base on the datasheet checking the recommended value and the typical design and I got resistor value in the hundred of kOhm who fit with the recommended value. 

Why Webench give me so high value?

Also, I try to edit the schematic with my own value to see the behavior of my circuit, but after finshing the edit, I lost all the simulation type (Bode Plot, steady state and transient).

Do we have a way to keep the simulation type with the edit design instead having the choice to plot only the probe?

Thanks