This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq80xRW OpenDevice in C#

Other Parts Discussed in Thread: BQPRODUCTION

Hi All,

I'm hoping this is going to be a no-brainer, but what I am trying to do is write an application in C# (MSVC 2010) using the bq80xRW OCX control that will control 4 EV2300s from a single application.  I've written a function in C# that will successfully open a single EV2300, but seems to stumble when trying to open more than one...

The code is:

        public bool connect(int index = 0 )
        {
            int gotten = 0;
            string boardNames = "";

            if (connected)
                return true;

            myBoard.GetAllBoards(4, ref gotten, ref boardNames);

            if( gotten < index + 1 )
            {
                return false;
            }

            string[] boardList = boardNames.Split(',');
            string board = boardList[index];

            int error = myBoard.OpenDevice(ref board);

            if( error != 0 )
            {
                return false;
            }

            connected = true;

            return true;
        }

So, what happens is:

The call to GetAllBoards seems to only return the available boards -- ie, on the first call it lists 4 boards, on the second it lists 3 boards. It seems to do the same thing that a call to GetFreeBoards does.

The call to OpenDevice returns 0 (success) on the first call, but -1 (fail) on the second call.

Anyone have any thoughts?

Does anyone have a decent SDK reference for the OCX control?

Thanks much,

Brian LeLacheur