This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3150 EVM board, Current limit

Other Parts Discussed in Thread: LM3150

Hi,

I am using LM3150 EVM board (500kHz) to build a buck converter from 20V to 14.5V. I changed the feedback resistor, inductor, output capacitors and Ron based on my application.  Everything works fine.

But I tried to test the current limit, it didn't work. I want  the current limit is between 3A and 4A. Based on the equation in the datasheet, I pick Rlim about 300 ohm, 250 ohm, 200 ohm. None of them work. Did I miss anything?

Thanks,

BM

  • Hi Botao,

    Thank you for the question. We will get back to you soon.

    Thanks,
    Anston
  • Hi Botao,

    Assuming you need Current limit at 3A and you are designing your supply with 20V in 14.5V@2.5A specs (Inductance at 10uH for 30 percent ripple) . The Rlim resistance for typical application comes out to be close to 250 ohm .

    Have you tried increasing the load and see where current limit kicks in . Also please share your updated schematic too .

    Ambreesh
  • Hi Ambreesh,

    Thanks for your replay. In my setup, the inductance is 10uH, the output capacitance is 20 uF. and the switching frequency is 250 kHz. Now I changed the Rlim to 100 ohm. I can observe the current limit triggered around 2.5A. 

    Why is there so much difference in Rlim between the calculated value and experimental value?

    Thanks,

    BM

     

  • Hi Botao,

    In the datasheet ,Rdson max is taken for the calculation , which results in higher value of Rlim as current limit kicks in if the voltage across
    RLIM and the voltage across the low-side FET are equal ( current limit comparator will terminate the next on-time cycle). This is done because even in higher temperature (where Rdson increases), the solution should be able to provide required current without hitting the current limit .

    With Regards
    Ambreesh