Hello,
i have problems to calibrate the Qmax of the battery.
I use the bq34z100 with bqStudio 1.3.45 and the Charger is a bq24170.
The Battery properties are:
7Cells parallel Panasonic NCR18650B.
Capacity: 22.4Ah
Energy: 82.2Wh
At the beginning I have calibrated the offset of the board and set the Chemistry-ID to 2012.
Configuration of the FuelGauge:
Taper current: 224mA
Design Capacity: 22400 mAh
Design Energy: 8220mWh
Design Energy Scale: 10
For calibrating the battery, i was using the following steps:
1. Send an IT Enable (21) command to turn ON FETs. Send a Reset command (41) to disable Ra-table updates.
2. Discharge to empty
3. Wait until the OCVTAKEN flag turns red.
4. Send IT Enable command to set a DOD0 reference point.
5. Charge to full (FC bit set.)
6. Wait until the OCVTAKEN flag turns red. You should see VOK turn green after Qmax has learned. You should see Update Status change to a 05.
7. Discharge at a C/8 rate down to Term Voltage.
8. Wait until the OCVTAKEN flag turns red. You should see Update Status change to a 06 during the rest period.
But on step 3 the OCVTAKEN flag doesn´t go to red and the RUP_DIS, QEN flags are red and VOK is green.
I am waiting for 8 hours and there are no changes.
What is the problem?
Thanks for help,
Daniel