THE SETUP: I have wired a TPS61222 circuit, as shown in Figure 26 of the data sheet (SLVS776B, REVISED NOV. 2014). The inductor is 4.7uH, and the caps are both 10uF. For testing, I am using a 560 Ohm resistor to simulate the actual load. This draws about 8.9 mA from the output.
THE PROBLEM: If I power up the circuit with the load in place, the output does not regulate to 5V. Varying the input from 2.5 - 5.0V provides an output of 3.5 - 4.5V.
I can then cause it to go in to regulation by removing and re-applying the load. Or, if I power it up WITHOUT a load, and then apply the load, it works fine.
Is this behavior normal for this chip? Any suggestions will be appreciated.
Thanks,
Ray