This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Requesting Part suggestion

Hi,

I am looking for a single cell Li-ion Battery charger with integrated fuel gauge. The specification are

  1. Max charging current- 2A
  2. Output voltage- 4.2V or 4.35V(preferred)
  3. Input Voltage- 5V nominal (from AC adapter)
  4. Control Interface-  I2C, SPI
  5. Battery capacity >= 6000mah 

Regards

Rakesh