Hola,
I'm using LM27313 as new project design as below circuit:
USBVCC is the power supply from NB, but the newest NB USB specification is 5V/1000mA and that will causes the output power increased from 6V/400mA
to 6V/1000mA so the LM27131's temperature will rising to 70'!
My question is that how can I limited the output current fixed at 500mA with this circuit?Can I use LM317 to limited the output current?if yes, how can I integrated
them?