Hello,
please help us to overcome an issue...
We use pin 3 (UDIM) in regards to PWM dimming - it works. Besides, the implemented circuit is identical to application note in datasheet.
Problem:
Additionally we use pin 6 (IADJ) to implement thermal pullback in case of elevated ambient operating temperatures.
The corresponding circuit is:
pin 5 (VREF) - 15k - PTC - pin 6 (IADJ) - 10k - GND
Besides - the PTC is a 110°C component with a resistance of 680Ohm before .
The issue is that this kind of thermal pullback doesn't have any effect on the LED current although the voltage on pin 6 (IADJ) is changing due to the PTCs resistor change at elevated temperatures.
QUESTIONS:
Can anybody advise us please so we can overcome the issue?
What is the switch "PWM_DIM" for ... on the OTA output (pin 6 IADJ) ? (Refer to page 10 of TPS92640 datasheet)
Any known issues regarding thermal pullback implemented in that way?
Thanks
Erwin