Hi,
I have card using the LMZ30606.
in the card I have functional problem - vout didn't stablize and the value is not as define.
I attached the schematic.
Pls. check it and advise.
Regards
Zeev Gerber
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have card using the LMZ30606.
in the card I have functional problem - vout didn't stablize and the value is not as define.
I attached the schematic.
Pls. check it and advise.
Regards
Zeev Gerber
Zeev:
The schematic was reviewed on both 1.5V and 3.3V LMZ30606. It was indicated there is instability on one or both Vout buses.
Electrical characteristic data page 5 on external output capacitors lists maximum total output ceramic capacitance of not more than 650uF. It also in note 6 and7 refer to a table 3 and table 5 for more details.
I recommend the removal of 1-100uFceramic on each output voltage bus, replacing it with a 100-220 polarized capacitor( ESR ≤ 25m ohms as described in table 5 and output capacitance note page 10.
The schematic is marked up with this suggested change.
Tom