E2e,
We have a customer that has designed in the TI TPS92512HV and have been experiencing some odd start up behavior that they would like to prevent if possible.
If PWM is high (5V) when the IC is turned on the unit pounds the LED with an initial current of 2A. It will then immediately recover and find its set current but this equates to a flash of light at start up, as well as stress to the LED.
Items to note.
1) Comp pin cap is .01uF this was necessary to prevent a turn on hiccup the unit did when PWM was brought from 0 to 1%
2) Switching frequency is set to 300K this also prevented some plashing we were experiencing due to possible min or max duty cycle issues.
3) output capacitance is 3uF and output inductor is 33uH
4) Max current is set to 1.44A
This flashing means they cannot use this part in analog applications.
How can this condition be eliminated?
Thanks for your help.
Regards,
John Wiemeyer