This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

50 watt led driver using lm3447

Other Parts Discussed in Thread: LM3447, STRIKE

hi sir ,

our design led driver 50watt using lm3447

and we ask about tvs diode rating standard for switching if we operated with transformer which

primary side N1 :7TS AND N2: 16TS  our input voltage 250vac maximum 

please send me your mail to send details data about our design 

best regards 

eng riad

  • Hello eng riad,

    I would like to get more information.  From this email I'm guessing that your transformer ration from primary to secondary is 7 turns to 16 turns?  Can you verify this?  At 250 VAC the peak input voltage is 250V * 1.414 = 353 volts.  At 7 to 16 that would equal -807 volts (this is why I ask).  The secondary side rectifier would have to be rated to 807 volts + the output voltage + any ring voltage which I would guess would need rating over 1000 volts.

    I would guess the TVS diode you are talking about is the primary side clamp for the leakage inductance?  The power rating of this depends on the output power but more important the transformer design.  If the coupling of the primary to secondary is poor the TVS clamp will have to dissipate a lot of power.  If the coupling is good the clamp may still need to dissipate up to five watts depending on operating conditions.  There are also other ways to clamp the MOSFET drain during MOSFET turn-off.

    It would be good to get a lot more information about your design.

  • hi sir ,

    nice to contact with you 

    as describe before we design our circuit by your company web design tool using lm3447 

    and creating design as tool but we found that tvs diode is heated driver_50w__10_1_2016.pdf80104563-EF25 MAIN TRANSFORMER.pdfLM3447_Design_Tool_sluc365_____zaki_30_9_2015___unprotected_using_password_3447.xlsxas description circuit 

  • Hello,

    Your transformer turns ratio is 62 turns to 16 turns, or 3.875:1. At 32 volts output, plus diode drop, the reflected voltage will be about 128 volts.

    The transformer specification has the primary inductance at 250 uH and the leakage at 30 uH. The drawing shows how the transformer is wound and I expect the leakage is much lower. It will not work well if the leakage is 30 uH so I would get the manufacturer to tighten up this specification. A very good coupled transformer approaches leakage inductance 1% of primary inductance though that is not necessary.

    The transformer is on the small side resulting in a fairly large gap (AL is low for that core size). This is due to designing a higher power flyback than the tool intended. It could work okay but just know the gap is large and there may be fringing heating depending on how the transformer is constructed.

    A SMA transient suppressor is much too small for the leakage energy to be dissipated, this TVS diode would be for a 7-10 watt design, not a 50 watt design. This is a discontinuous mode operation which is the worst case for a flyback design in regards to leakage energy dissipation.

    You could measure the leakage inductance of the transformer just how they state in the transformer datasheet to verify the leakage inductance (and also measure the inductance with all windings open for the primary inductance). You could then calculate how much the clamp must dissipate though you need to understand the math. Another method would be to replace the 170 volt TVS with something like six 30 volt TVS diodes in series. You could measure the temperature rise and then compare this to running a small DC current through the TVS diodes to reach the same temperature to get approximate power dissipation in the clamp.

    I'm sure the SMA transient suppressor is heating up at this power level and type of flyback. It needs to be able to dissipate much more power than the SMA size package.

    Thanks,
  • im sorry for late
    first we ask about how to measure leakage inductance of transformer which is contain of secondary coil and auxiliary coil and primary coil
    second we ask also about TVS diode we change tvs 170 voltage with TVS SMCJ200A clamping voltage is 324v
    and remain the same result TVS heated and burned
    so we ask about are any other parameter unlike spike of voltage will affected on TVS DIODE
    third : we try to measure the inductance of transformer we found that :
    1- primary coil inductance L(1,2): 0.256mh
    2- auxiliary coil inductance L(4,5): 0.00405mh
    3- secondary coil inductance L(10,9): 0.018mh
    all measure with open circuit
    4- when short circuit between (4,5)pin and (10,9) and measure leakage inductance
    we found that L(leakage inductance) (1,2):0.033mh
    and when all pin (4,5,9,10) and measure leakage inductance L(1,2): 0.0708mh
    this is parameter that your request before
    please advice me
    thank you
  • im sorry for late

    first we ask  about how to measure leakage inductance of transformer which is contain of secondary coil and auxiliary coil and primary coil

    second we ask also about TVS diode we change tvs 170 voltage with TVS SMCJ200A  clamping voltage is 324v

    and remain the same result TVS heated and burned  

    so we ask about are any other parameter unlike spike of voltage will affected on TVS DIODE      

    third : we try to measure the inductance of transformer we found that :

    1- primary coil inductance L(1,2): 0.256mh

    2- auxiliary coil inductance L(4,5): 0.00405mh

    3- secondary coil inductance L(10,6): 0.018mh

    all measure with open circuit

    4- when short circuit between (4,5)pin and (10,6) and measure leakage inductance

    we found that L(leakage inductance)   (1,2):0.033mh

    and when all pin (4,5,6,10) and measure leakage inductance L(1,2): 0.0708mh

    this is parameter that your request before

    please advice me 

    thank you  

    sorry for 

  • im sorry for late

    first we ask  about how to measure leakage inductance of transformer which is contain of secondary coil and auxiliary coil and primary coil

    second we ask also about TVS diode we change tvs 170 voltage with TVS SMCJ200A  clamping voltage is 324v

    and remain the same result TVS heated and burned  

    so we ask about are any other parameter unlike spike of voltage will affected on TVS DIODE      

    third : we try to measure the inductance of transformer we found that :

    1- primary coil inductance L(1,2): 0.256mh

    2- auxiliary coil inductance L(4,5): 0.00405mh

    3- secondary coil inductance L(10,6): 0.018mh

    all measure with open circuit

    4- when short circuit between (4,5)pin and (10,6) and measure leakage inductance

    we found that L(leakage inductance)   (1,2):0.033mh

    and when all pin (4,5,6,10) and measure leakage inductance L(1,2): 0.0708mh

    this is parameter that your request before

    please advice me 

    thank you  

    sorry for 

  • Hello again,

    I did the math to calculate the power dissipation for the clamp.

    If the leakage inductance is 0.033 uH and the primary inductance is 0.256 uH the power dissipation for the clamp would be around 7 watts.

    If the leakage inductance is 0.0708 uH and the primary inductance is 0.256 uH the power dissipation for the clamp would be around 15 watts.

    The SMA package can only dissipate approximately one watt depending on how well it is thermally connected to the board.

    Leakage inductance that high is bad for a flyback converter.  Looking at the transformer drawing, if it is built that way, I don't think the leakage would be that high but I have seen it too high because it doesn't match the drawing.  The secondary between the two primary windings is good.  They also need to lay over each other.  If they didn't evenly split the winding to have good coupling (how the secondary lays over the primary on the bobbin, the coupling gets worse, this increases the leakage inductance.

    Regardless, at 50 watts the clamp needs to dissipate more power than what you have for a clamp.  Moving the clamp voltage up will only slightly affect the energy because it's trying to clamp the leakage energy of the transformer which is from an inductor.  I would try, like I said before, placing five 33 volt TVS diodes in series for the clamp to see if that works, that allows up to five watts of dissipation (again depends on heatsinking the parts).  If it is still too hot I would investigate the transformer manufacturing since the leakage must be too high.  Leakage loss will directly affect the efficiency of the converter.

  • hello sir ,

    all value in mele Henry not micro so

    1- primary coil inductance L(1,2): 0.256mh    NOT MICRO BUT mele henry 

    2- auxiliary coil inductance L(4,5): 0.00405mh    NOT MICRO BUT mele henry 

    3- secondary coil inductance L(10,6): 0.018mh       NOT MICRO BUT mele henry 

    all measure with open circuit

    4- when short circuit between (4,5)pin and (10,6) and measure leakage inductance

    we found that L(leakage inductance)   (1,2):0.033mh  NOT MICRO BUT mele henry

    and when all pin (4,5,6,10) and measure leakage inductance L(1,2): 0.0708mh    NOT MICRO BUT mele henry

    im sorry for more indication

    best regards

    eng riad  

  • Hello,

    Units are correct, mH is millihenry, uH would be microhenry per how I use the units.  I also calculated the operation of the transformer separate from the design tool and the peak current is very similar so I know the units are correct.

  • hi sir ,

    thank you very much 

    i understand that all answer before well for us right 

    kindly we need to know  about the math calculation power dissipation of clamp

    and what about TVS diode SMCJ200A that power 1500watt

    and also heating

    best regards

    eng riad 

  • hi sir ,
    im dont understand you about the calculation power dissipation are equal regardless unites mili or micro
    please more details about your math
    im very sorry but exactly not understand
    best regards
    eng riad
  • Hello,

    TVS diode SMCJ200A is a transient suppressor. It is rated for 1500 watts peak for a surge event (not used that way here). It is rated for 1500 watts peak. There is also a continuous rating if it has a proper heatsink. One datasheet states 6.5 watts on infinite heatsink. In reality, on a PCB board, the continuous rating will be two watts maximum but probably more like one watt if you include your products operating temperature range. Like I said before, try taking five or six SMCJ33A in series and try to see if it still runs too hot. They will need some form of heatsinking. They also make these in through hole parts if you just want to test it. At 50 watts the clamp will need to dissipate much more than one watt and if only one SMCJ200A is used it will get too hot.
  • Hello,

    I did this outside of the design tool to figure out how much energy the TVS clamp will need to dissipate based on your transformer measurements, I used the two different leakage numbers you provided.  The leakage is high so the clamp needs to dissipate quite a bit of power.  Vout is 33 because of the added diode drop.

    I calculated at the peak of the rectified AC and then divided by two to get the PFC power dissipation in the TVS clamp.

    Ipripeak is very close to what the tool calculates.

  • hi sir ,

    thank you for your help us in our design 

    we will make a series of tvs diode as you say

    but we found that there are several type of tvs that name of SMCJ33A  which clamping voltage between 53v------69v and maximum peak pulse current between 28A ------100A----104A which one can chose to buy 

  • hi sir ,

    we wait you to tell us what about  several type of tvs that you advise us 

    thank you 

  • Hello,

    Sorry, I was out for a few days.  You can use the same family as the SMCJ170 you are using.  The clamp voltage on the datasheet is for high current (surge suppression).  In your application the current is not that high so it will clamp above the It current spec, same as the SMCJ170 (or 200) that is running too hot.  The peak current the clamp will see is the same as the peak current calculated for the design, around 3.5 amps.

  • hi sir ,

    im sorry for tired you 

    ask about tvs smcj33a that you  advise me but it also clamp at peak current 28 ampere and you say current is around 3.5A 

    are the difference between the two current will affect on behavior of operation

    best regards

    eng riad  

  • Hello,

    The current rating for a TVS is for a surge event.  The TVS in your circuit is being used in a different manner than original intent.  A TVS is a sort of Zener diode that can handle large pulses of current/energy.  It is used to clamp voltages of circuits during a surge event such as a lightning strike.  This prevents overvoltage of components in a circuit. 

    In your application you are using it as a zener diode than can handle large pulses of current.  At 200 volts and 3.5 amps of current that is 700 watts.  This is for a very short time so the average power is much much lower.  The current rating does not matter in this application as long as it is above what the leakage current spike is, 3.5 amps.  The problem you are running into is the average power.  The SMC package is capable of one to two watts if mounted on an FR4 board.  Your leakage energy average is more than this and why the part is running too hot.  Trying five SMCJ33 parts allows five times the power dissipation.  It may still not be enough in your case especially if the transformer is not optimized to reduce leakage inductance.

  • hi sir ,

    when measure the leakage inductance L(2-1) was two case :

    1- when make separate short circuit on each (aux , secondary )  leakage was 33uh and ratio between the leakage inductance(33uh) to primary inductance (250uh) was about 12%

    2- when make  short circuit on each (aux , secondary )  and short circuit between the aux and secondary

    (short circuit all pin aux-secondary)

    leakage was 70uh and ratio between the leakage inductance(70uh) to primary inductance (250uh) was about 27%

    im sorry we will try you suppose about five tv smc33A but i think that all information about the measurement not clear so 

    ask you in the first measure leakage inductance was about 12% primary inductance  is this suitable for us or not 

    and second measure which leakage inductance was about 27% primary inductance is this correct measure or not

    im sorry for tired you but we want to understand because you say before that leakage inductance must be equal to 1% not exceed and when read document about the transformer we found also  leakage inductance must also within (2-4)% primary inductance 

    best regards 

    eng riad

                  

  • Hello,

    I don't think your leakage measurements are correct but if they are you will have to dissipate a lot of power in the TVS clamp circuit.  This is something you have to work with the transformer manufacturer.  I would take one apart to see how the winding fit next to each other but in you case I would just try the five SMCJ33s in series to see if it still runs too hot or not.

    The leakage inductance does not need to be 1% or less, that would be ideal.  The higher it is the more power needs to be dissipated in the clamp.  It will also affect the efficiency.

  • hi sir ,

    thank you very much we will test five tvs in series as you tell us 

    second we ask about our application is non dimming and after read data sheet lm3447 that recommended pin FLT2 will connected to pin  TSENS but when insert prameter to tool will give connected pin FLT2with low pass filter pin FLT1

    what about confusion of us and is this dimming affect on the too heat in tvs diode or not

    finally if we want non dimming operation what pin connected to of PIN (TSENS- FLT1- FLT2)  

    THANK YOU VERY MUCH 

  • Hello,

    If you are not using TSENS you can connect TSENS to FLT2 and remove the low pass filter connected on FLT1 that goes to FLT2.  FLT1 is an output that is low pass filtered and an input to FLT2 as a DC level to set dimming based on the angle detected from the AC line (In a triac dimmed application).  You could just leave the dimming circuit as is and it will never decode dimming because there is no triac present on the input.

    If you are using TSENS (with an NTC thermistor) I would not connect FLT2 to TSENS since it will start to dim earlier due to FLT2 input range.  NTC foldback starts at 1.0 volts and FLT2 dimming starts at 1.45 volts.  If there is no NTC connected TSENS is at 1.75 volts which allows full output power since it is above 1.45 volts.

    If you are unsure, just leave the RC on FLT1 and the filtered signal connected to FLT2.  It will operate at full power since the angle detect will not sense a triac signal.

    If you are dimming the TVS will dissipate less power but if the LED driver is putting out 50 watts, regardless of how the FLT2 and TSENS pins are connected the TVS will dissipate the same.

  • hi sir,

    thank you for reply me we also want what exactly the function of dimming to decided use it or not and what prefer of in starting experiments led driver 50 watt or what is the sequence in test to driver or steps  to protect our driver from burned

    thank you very much

    eng riad     

  • The LM3447 is intended to be used with interfacing to triac dimmers.  If there is no triac dimmer it will function as a non-dimming LED driver.  I gather that you are not using this for triac dimming and it will work for that.

    To try and prevent board failure during testing due to hot parts you could reduce the output power to start out.  This way you can make sure everything is working correct.

  • hi sir ,

    nice to contact with you again 

    we test circuit with your suggest with five tvs SMCJ33A in series and test we found that all heating so we increase number of it to reach 8 tvs smcj33a so we found that temperature are high but no as 5 tvs temperature reach to 62c and no fault found until now and operated time about one hour this is  result is good for us compare with one tvs smcj200A what about your opinion in this result and we also try to minimize the number of tvs by search another tvs  advise me if possible

    second we ask you about the EMI FILTER

    we found that when circuit operated with emi filter we found that Rsnub is very heated and design tool tell us this resistance is

    pulse withstanding what the difrence between the normal resistor and this pulse resistor and tool tell us this resistor tuning from (220------1200)OHM  what equation about this to calculate the exact value

      third : we try to found the best transformer that leakage inductance about 2----4% to give the best result what are about your opinion      

    best regards 

    eng riad 

  • hi sir ,

    nice to contact with you again 

    we test circuit with your suggest with five tvs SMCJ33A in series and test we found that all heating so we increase number of it to reach 8 tvs smcj33a so we found that temperature are high but no as 5 tvs temperature reach to 62c and no fault found until now and operated time about one hour this is  result is good for us compare with one tvs smcj200A what about your opinion in this result and we also try to minimize the number of tvs by search another tvs  advise me if possible

    second we ask you about the EMI FILTER

    we found that when circuit operated with emi filter we found that Rsnub is very heated and design tool tell us this resistance is

    pulse withstanding what the difrence between the normal resistor and this pulse resistor and tool tell us this resistor tuning from (220------1200)OHM  what equation about this to calculate the exact value and if there are tool to calculate emi filter please advise me 

      third : we try to found the best transformer that leakage inductance about 2----4% to give the best result what are about your opinion      

    best regards 

    eng riad 

  • hi sir ,

    nice to contact with you again

    we test circuit with your suggest with five tvs SMCJ33A in series and test we found that all heating so we increase number of it to reach 8 tvs smcj33a so we found that temperature are high but no as 5 tvs temperature reach to 62c and no fault found until now and operated time about one hour this is result is good for us compare with one tvs smcj200A what about your opinion in this result and we also try to minimize the number of tvs by search another tvs advise me if possible

    second we ask you about the EMI FILTER

    we found that when circuit operated with emi filter we found that Rsnub is very heated and design tool tell us this resistance is

    pulse withstanding what the difrence between the normal resistor and this pulse resistor and tool tell us this resistor tuning from (220------1200)OHM what equation about this to calculate the exact value

    third : we try to found the best transformer that leakage inductance about 2----4% to give the best result what are about your opinion
  • Hello,

    Increasing from five 33 volt TVS to eight 33 volt TVS diodes not only adds three more parts for power dissipation but there will also be less dissipation in the clamp due to higher voltage, 5 X 33 versus 8 X 33.  There are other methods to clamp and burn the leakage energy such as a diode, capacitor and resistor.  More important though is how much you have to dissipate in this clamp.  A discontinuous flyback requires the transformer be wound to keep the leakage inductance low.  I would look at the transformer design to see if you can lower it significantly.  I don't know how much power you are burning in the 5 X 33 volt TVS diodes but if it's a watt each the leakage is going to be responsible for about 10% of your efficiency loss.  It would be best to try and reduce it more if possible.  What I do is take one of the transformers and take it apart to see how it is manufactured.  If you know what you are looking for it becomes apparent if the windings are coupled well or could be improved.


    Rsnub.  I'm assuming this is the damper for the triac dimmer, R17 and R2?  With a 1 uF damper capacitor at 265 VAC input (high line) and 60 Hz (worst than 50 Hz) the resistor will need to dissipate 1/2*C*V^2*(60Hz*2) which is over eight watts during triac dimming.  It will also need to dissipate around four watts continuous from the AC input waveform.  The resistor, if 390 ohms, needs to be able to handle pulse power rating of 375^2/390 = 360 watts (V^2/R).  This is the minimum pulse rating of the resistor, I would much higher to prevent damage from surge events.

    Power rating for resistor needs to be over 12 watts continuous, 360 watts peak rating if using 390 ohms.  In the application it will be lower but an equation really doesn't help with this since it's related to any triac dimmer you connect to the input.  This, unfortunately, requires testing with many triac dimmers to see what the input current to the power supply looks like when triac dimming using all the available triac dimmers you want to be compatible with.  The resistor value will be much lower than 390 ohms.  That value is more optimum for a much lower capacitor value such as 0.1 uF to 0.33 uF.  The pole frequency will be lower if the capacitor is 1 uF and the idea is to try and damp the input current waveform from the resonance the triac rising edge causes with the LED drive EMI filter (mostly the X-capacitor).  I would revisit the EMI filter to possibly add another LC set so the values can be reduced.

  • hi sir ,

    nice to contact again 

    remember me about the design 50watt led driver using lm3447 

    we were face a big problem about the the TVS diode that it was heating and over come this problem by connecting series tvs diode 

    after finish our design we found that all efficiency of driver about 73% this ratio is very low 

    how can solve this problem to increase efficiency to 90% 

    thank you very much 

  • Hello,

    73% is low.  Normally a lot of this would be known during the design cycle when calculating for all the component values and the transformer.  There are many areas that can dissipate additional power.  The easiest method to figure it out now would be a thermal camera to see what is dissipating power.  Some of the areas I would check are the MOSFET, the main output rectifier, the transformer, the leakage clamp circuit and for incorrect operation.  It can be a combination of things causing low efficiency.


    Thanks,