Other Parts Discussed in Thread: BQ51003
I use the EVM board to test. When the distance between RX-COIL and TX-COIL is about 1.5mm or little than 2mm, it can not charge. Even when I close the FOD function.
The EVM board is BQ500212A-EVM.But the receiver is our product. The RX coil is TDK's WR221230-36M8-G, and the TX coil is custom-made(φ30.0).The tx coil is bigger than rx coil. And the rx coil is rectangle.