This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Charger Supplement Mode

Hi Team,

I see that supplement mode is used to temporarily have the battery provide additional power to the system when the system's peak power is higher than the input power (and with the charge current already reduced to 0A).  My question is - is supplement mode limited to NVDC chargers only?  Is DPPM mode also required?

Thanks in advance for your support.

Best Regards,
Brian Gosselin

  • No. If you have a non-power path charger, with the system tied to the battery tied to the output of the charger, the battery will help provide any system transients that exceed the input power limitations of the charger.