This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

2S-3S USB BALANCE CHARGER

I am planning to design 2s-3s USB balance charger for LI-PO with the following specs

  • Input is 5VDC (0.9-3.1A)
  • Automatically sense if 2S or 3S is connected to the onboard JST XH connector and provide 4.2VDC (balancing available current) between each cell.
  • Provide balance charging – charging and discharging each cell until an even charge is achieved across all cells.
  • LED indicator (red/green) to indicate charging status.
  • Include one-way diode to prevent reverse drain in the event of malfunction from external power source. (eg: wall plug/car adapter)

can anyone provide any help or a design using available chips?