Hi,
I recently set up a power supply for the conversion of 400V...900V DC into 24V DC with a nominal power of 120W.
I am using a UCC28712 IC with a standard flyback configuration.
My Transformer has a primary inductance of 950µH and a turns ratio of 12.
Yesterday I ran the power supply at nominal power at 400V...900V.
Unfortunatelly the IC will not go to 100kHz.
My first configuration is:
Rcs=500mOhms, Peak-Primary-current=1,56A (@Vcst=780mV)
The converter will switch at about 60kHz with Vcst=750...800mV.
The secondary voltage goes only to 20V (Feedback voltage at VS-pin is about 3,5V)
The converter Switches in the 4th or 5th valley of the Drain-Source-Voltage and does not go up.
Then I reduced the Rcs to 330mOhms (Peak-Primary-current=2,36A)
This means more energy is transfered to the Output per pulse.
The converter then brings the Output to 24V as intended.
Feedback-Voltage at VS-pin is about 4,1V.
Peak-Voltage at CS-Pin is about 750...800mV.
The converter runs at a switching frequency as low as 30kHz.
In this working Point my Transformer, Mosfet and Output-Diodes overheat because of the high Peak-currents.
How do I get the converter running at 100kHz as intended?
Kind regards
Sven