Is anybody familiar with non-spec compliant PoE PSE?
Generically speaking the term is "dirty PoE". So far as I can tell it is a class of products that exists that provides 12-24VDC over either the primary or spare pairs of an RJ-45. This voltage is provided continuously. No negotiation, no recognition of classification resistors. Not much to do with the PoE spec. Just a DC supply cabled over RJ45. Here is an example:
At any rate I'm working on a design with TPS23753A. Anyone have insight on how to accommodate this type of PSE? The best idea I have thus far is somehow route the dirty PoE over to the auxiliary power input and properly OR the device to have PoE preference. This way if a valid PSE is hooked up it will use it and show up correctly on network configuration tools. If the voltage is only 12-24VDC, the auxiliary input should take over and work.
Any thoughts? Anyone else looking into dirty PoE?
Thanks,
V